RELEASE NOTES PowerAlert Element Manager 1.0.0 (Build 266) 21-MAR-2021 SHA1 hash: 039f058a3a6723b54128cba7199653677cd34706 Copyright (c) 2021 by Tripp Lite All Rights Reserved IMPORTANT NOTES Malwarebytes antivirus may block PAEM connections if "Java Malicious Inbound Shell Protection" is enabled in Malwarebytes. Disabling" Java Malicious Inbound Shell Protection" has been confirmed to resolve the issue. For details on the false positive problem – which affects PAEM and other software using Java – see the links below: https://forums.malwarebytes.com/topic/252540-blocking-java/ https://forums.malwarebytes.com/topic/265625-java-rtp-detection-possibly-eclipse-related/ REQUIREMENTS DEFECT FIXES ENHANCEMENTS KNOWN ISSUES PAEM will not discover a device if it has SNMP disabled and its HTTP credentials are different from those entered in PAEM Log entry details insufficiently describe error codes and conditions During a firmware update, PAEM will ignore devices that are already running that firmware version User-customized views are not retained after navigating from, then returning to the original screen or after refreshing the screen PAEM does not display the quantity of devices undergoing a mass configuration operation Log entries insufficiently record the outcome of successful operations PAEM does not provide sufficient notification of successfully completed operations PAEM does not display network information pertaining to the system on which it is operating. Records of user login and logoff activity are not available in a viewable log An Application Log is not available in this release IP Binding is not available in this release HTTP to HTTPS Redirection is not available in this release Scan profiles cannot be independently selected or unselected when running a Scan Support of Safari OS is not available in this release The position of vertical scroll bar affects the position of displayed top menu sub-items The edit icon (pencil) overlaps IPv6 addresses in the "Add/Edit" Device Catalog window If the computer hosting PAEM is rebooted while a PAEM operation is in process, subsequent PAEM operations may not complete successfully. To resolve, run a Scan before executing the operation. Running Repair/Modify of the PAEM installation may fail if the entered port value is the same as the one currently in use. The workaround is to enter a different port. END RELEASE NOTES