Tripp Lite

News Release

Media Contact
Samantha Casey
Senior Digital Marketing Specialist
773.869.1258
samantha_casey@tripplite.com

Tripp Lite’s New Power Strips with USB Charging Mount without Tools or Fasteners

Included Clamps Enable Easy Access to Outlets and USB Charging Ports

Chicago, IL (September 16, 2019)—Tripp Lite, a world-leading manufacturer of power protection and connectivity solutions, has made it easy to mount its newest power strips for faster installation and improved access to AC outlets and USB charging ports.

The PSC240410USBB and PSC360610USBB feature heavy-duty C-clamps that mount to the edge of desks, tables and workbenches without the need for tools or fasteners. After the clamps are in place, the power strips simply snap into built-in clips on the clamps. The AC outlets and USB-A charging ports are grouped in pairs along the length of each strip, offering convenient access to power and mobile device charging, while reducing cord clutter.

“The clamps take the hassle out of mounting and relocating a power strip installation,” said Karenann Brow, Director of Product Marketing for Surge, Power Strips and Display Mounts. “These power strips are ideal for temporary installations and other situations where traditional wall mounting isn’t possible or convenient. The clamps allow customers to have power and charging within easy reach at their desktops.”

The mounting clamps are also sold separately in pairs for use with other Tripp Lite PS- and SS-series bench-mount power strips.

  AC/USB Power Strips with Mounting Clamps

Model PSC240410USBB

 

Learn More

Key Features of Tripp Lite Power Strips with Mounting Clamps

  • 24-inch or 36-inch strip with durable metal housing
  • NEMA 5-15R outlets (4 or 6) and USB-A charging ports (4 or 6)
  • 3.1A shared per pair of USB-A charging ports
  • Included steel mounting clamps with built-in clips; no tools required
  • Included surface-mounting clips for standard mounting
  • 10 ft. input power cord for placement flexibility
  • Lifetime warranty

Get more information about Tripp Lite’s full line of power strips at tripplite.com.

 

Share on LinkedIn Share on Twitter Share on Facebook

 


About Tripp Lite
Since 1922, Tripp Lite has established a global reputation for quality by providing reliable products and exceptional service to customers worldwide. From desktop to critical infrastructure, Tripp Lite products and solutions power and connect the computers, networking equipment and electronic devices that form the foundation of our digital world. Headquartered in Chicago, Tripp Lite manufactures UPS systems, cables, connectivity solutions, PDUs, racks, cooling solutions, KVM switches, console servers, charging stations, display mounts, surge protectors, power strips, network switches, power inverters and specialty products for data center, healthcare, government, education and digital signage applications. Learn more at tripplite.com.

Over 95 Years of Manufacturing Excellence
Tripp Lite

tripplite.com • 1.773.869.1776