|
Tripp Lite’s New Outdoor Wall Mounts Withstand the Elements
Customers Can Hang Displays Outdoors with Peace of Mind
Chicago, IL (October 12, 2020)—Tripp Lite, a global manufacturer of power protection and connectivity solutions, makes it easy to mount TVs and monitors outdoors. The rugged new DWM3270XOUT and DWM3780XOUT wall mounts are resilient against rain, snow, dust, sand, mold, mildew and salt spray, and are designed for permanent outdoor installation on patios, balconies, decks and outdoor spaces at bars and entertainment venues.
Built to accommodate 32- to 80-inch flat-panel and curved TVs and monitors weighing up to 110 lb., these electroplated mounts with powder-coated finish are VESA compliant for compatibility with most popular display mounting hole patterns. Their articulating arm and one-touch screen angle adjustment make it easy to create optimal viewing angles. Weatherproof flat-screen covers (sold separately) provide protection for the displays themselves, so customers can conveniently leave both their mount and their display setup outdoors with peace of mind.
“Customers looking for convenience with outdoor TV viewing will appreciate these new models,” said Karenann Brow, Director of Product Marketing for Surge, Power Strips and Display Mounts. “Tripp Lite’s outdoor articulating wall mounts are very much set-it-and-forget-it. Customers can skip the hassle of covering them or uninstalling them because of weather, and they’re easy to set up and adjust.”
|
|
|
|
|
Outdoor Wall Mount with Articulating Arm for 37 in. to 80 in. Displays
|
|
|
Key Features of Tripp Lite’s Outdoor Articulating Wall Mounts
- Electroplated frame with high-grade, powder-coated finish for outdoor use
- Stainless steel screws
- Articulating arm extends screens away from the mounting surface
- Accommodate 32- to 80-inch TVs and monitors weighing up to 110 lb.
- One-touch screen adjustment with -90 to +90° swivel, -20° to +10° tilt and -3° to +3° screen level rotation
- VESA compliant to accommodate a wide range of displays
|
|
|
|
|
|
|
|
|
|
About Tripp Lite Since 1922, Tripp Lite has established a global reputation for quality by providing reliable products and exceptional service to customers worldwide. From desktop to critical infrastructure, Tripp Lite products and solutions power and connect the computers, networking equipment and electronic devices that form the foundation of our digital world. Headquartered in Chicago, Tripp Lite manufactures UPS systems, cables, connectivity solutions, PDUs, racks, cooling solutions, KVM switches, console servers, charging stations, display mounts, surge protectors, power strips, network switches, power inverters and specialty products for data center, healthcare, government, education and digital signage applications. Learn more at tripplite.com.
|
|
|
|
|
|
|