|
|
Tripp Lite’s New HDMI Splitters Provide Multi-Resolution Output Support
Transmit Video and Audio to Multiple TVs with Different Display Resolutions
Chicago, IL (September 5, 2019)—Tripp Lite, a global manufacturer of power protection and connectivity solutions, has introduced HDMI splitters that give users the ability to take advantage of true 4K resolution on a newer 4K display, while still using other existing or less-costly screens displaying lower resolutions within the same installation.
Most other HDMI splitters default each display to the lowest common resolution of all connected displays. In contrast, these new solutions support multi-resolution output, so that 4K content is displayed at the maximum output supported by each television, monitor or projector.
“With one of these new splitters, the user gains a cost-effective means to install one or more televisions that support High Dynamic Range (HDR) for true 4K content, while controlling the overall costs of the installation by adding other displays that support 1080p resolutions,” said David Posner, Tripp Lite’s Director of Product Marketing, Connectivity. “The ability to mix-and-match different display standards means that dazzling 4K video won’t be choked back to 1080p on an HDR television that may serve as the centerpiece of a larger installation.”
|
|
|
|
|
|
Multi-resolution splitters are ideal for applications where content from one 4K source is shown simultaneously on two or more displays of different resolutions, such as in bars and restaurants, hotels, auditoriums, churches, schools and trade show venues.
These multi-resolution output splitters support HDR resolutions up to 4096 x 2160 at 60 Hz for crystal-clear true 4K video. They also support the latest HDMI standards, including 4:4:4 chroma subsampling and 36-bit Deep Color. A wide range of audio formats are supported as well, including DTS-HD, Dolby TrueHD, Dolby Digital Plus and LPCM 7.1-channel surround sound.
|
|
|
|
|
|
|
Key Features of Tripp Lite’s Multi-Resolution Output Splitters
- Enable an HDMI signal to be distributed to multiple displays of different resolutions, with the video shown at the maximum resolution available on each display
- Available in 2-port and 4-port models
- Extend signals up to 30 ft. (15 ft. from source to splitter and 15 ft. from splitter to display)
- Support for video resolutions up to 4K x 2K (4096 x 2160) at 60 Hz
- Backward compatible with 4K at 30 Hz and 1080p at 60 Hz
- Support for 4:4:4 chroma subsampling for compatibility with high dynamic range (HDR) displays
- Support for up to 7.1-channel surround sound audio
- Meet HDMI 2.0 and HDCP 2.2 standards
The new splitters join Tripp Lite’s already-robust selection of audio/video connectivity solutions. Get more information about Tripp Lite’s full line of splitters and switches at tripplite.com.
|
|
|
|
|
|
|
|
About Tripp Lite Since 1922, Tripp Lite has established a global reputation for quality by providing reliable products and exceptional service to customers worldwide. From desktop to critical infrastructure, Tripp Lite products and solutions power and connect the computers, networking equipment and electronic devices that form the foundation of our digital world. Headquartered in Chicago, Tripp Lite manufactures UPS systems, cables, connectivity solutions, PDUs, racks, cooling solutions, KVM switches, console servers, charging stations, display mounts, surge protectors, power strips, network switches, power inverters and specialty products for data center, healthcare, government, education and digital signage applications. Learn more at tripplite.com.
|
|
|
|
|
|
|