|
Tripp Lite’s Isobar Premium Surge Protectors Now Available with USB Charging Ports
The Gold Standard for Surge Protection Offers New Functionality
Chicago, IL (December 21, 2018)—Tripp Lite, a global manufacturer of power protection and connectivity solutions, has expanded its line of Isobar® premium surge protectors to include models with USB‑A charging ports. The new models bring the convenience of USB mobile device charging to the most popular four- and six-outlet configurations of the Isobar, the gold standard for surge protection.
The new IBAR4ULTRAUSBB and IBAR6ULTRAUSBB surge protectors have widely spaced NEMA 5-15R outlets with the same robust surge-blocking architecture as other Isobar models to deliver reliable protection against AC voltage surges and spikes. If the protection circuit is incapacitated, an automatic shutoff feature permanently cuts power to the outlets to protect connected devices. Isobar models also have isolated filter banks to provide noise filtering between devices connected to the same surge protector.
Two USB‑A charging ports share 3.1A for charging smartphones, tablets and other USB mobile devices. The USB ports eliminate the need for an AC adapter for charging cords, leaving more outlets available for plugging in AC equipment.
|
|
|
|
“Isobar is an icon in our industry, so adding USB charging ports elevates an already premium product to the next level,” said Karenann Brow, Director of Product Marketing for Surge, Power Strips and Display Mounts. “Tripp Lite has taken the same Isobar surge protectors that customers have trusted for years and provided a convenient option for charging mobile devices.”
The new Isobar models have a metal housing with a black finish to complement most office equipment. Both models have a right-angle NEMA 5-15P plug to require less clearance between furniture and wall outlets. Keyhole slots on the back panel support wall-mount installation.
|
|
|
|
|
|
Key Features of Tripp Lite’s Isobar Premium Surge Protectors with USB Charging
- Four or six NEMA 5-15R outlets with isolated filter banks
- Surge suppression rating of 3330 or 3840 joules
- Two USB-A charging ports (3.1A shared)
- Combination AC circuit breaker and illuminated on/off switch
- Diagnostic LEDs (protection, fault and line status)
- 8 or 10 ft. input power cord with right-angle NEMA 5-15P plug
- Durable metal housing with black finish
- Lifetime limited warranty
- $50,000 connected equipment insurance
|
|
Get more information about Tripp Lite’s full line of Isobar premium surge protectors at tripplite.com.
|
|
|
|
|
About Tripp Lite Outstanding product reliability and exceptional service have been Tripp Lite trademarks for over 95 years. Tripp Lite´s innovations include the world’s first UPS system designed specifically for personal computers and the world’s most trusted premium surge protector—the Isobar®—with more than 19 million in use. Tripp Lite maintains the highest level of ready-to-ship inventory in the industry with more than 4,000 different products, including UPS systems, rack systems and cooling solutions, PDUs, PowerAlert® software for enterprise-level system management and control, surge protectors, KVM switches, cables and connectivity products, inverters, power strips and notebook accessories. Headquartered in Chicago, Illinois, Tripp Lite maintains a global presence with fully staffed offices worldwide. Additional information, including a list of Tripp Lite’s sales offices and authorized reseller partners, can be found by visiting Tripp Lite’s website: www.tripplite.com.
|
|
|
|
|
|
|