Tripp Lite

News Release

Media Contact
Autumn James
PR/Media Specialist
Tripp Lite
773.869.1229
autumn_james@tripplite.com

Tripp Lite’s Hospital-Grade Locking Power Cords Help Prevent Accidental Disconnection

Locking C13 Connector Provides a Strong Hold to Keep Equipment Powered

Chicago, IL (October 23, 2018)—Tripp Lite, a world-leading manufacturer of power protection and connectivity solutions, has expanded its line of hospital-grade power cords to include locking cords that resist accidental disconnection.

The new cords have a locking C13 end that connects to the C14 power inlet on computers, scanners, lab equipment, mobile carts and other hospital equipment outside the patient care vicinity. The locking feature provides a strong hold to prevent the cord from coming loose due to vibrations or unintentional pulling. Both slide buttons must be retracted to release the connector. The locking connector ensures equipment stays powered, preventing the expense and inconvenience of unplanned downtime.

The input end of the cord has a hospital-grade NEMA 5-15P HG plug for connection to a grounded hospital-grade AC outlet.

“Healthcare environments require reliable power connections for uninterrupted operation,” said Jim Folk, Tripp Lite’s Director of Healthcare Solutions. “The locking mechanism on the C13 connector makes these cords ideal for equipment that is frequently repositioned, especially in server racks and other tight spaces.”

Locking Hospital-Grade Power Cables

Learn More

Download Product Images

Key Features of Tripp Lite’s Hospital-Grade Locking Power Cords

  • Locking C13 connector provides a strong hold to prevent accidental disconnection
  • 10A cords are available in lengths up to 15 ft. (4.6 m) to provide flexibility in equipment placement
  • 15A, 25 ft. (7.6 m) cord is available for devices requiring a heavy-duty power cord
  • Tested to ANSI/UL 62 and 817 and CAN/CSA C22.2 no. 21 and 49 to safely provide power outside the patient care vicinity
  • Suitable as replacements for standard power cords in hospitals, clinics, medical offices and long-term care facilities

Get more information about Tripp Lite's full line of healthcare solutions at tripplite.com.

 

Share on LinkedIn Share On Twitter Share On Facebook

 


About Tripp Lite
Outstanding product reliability and exceptional service have been Tripp Lite trademarks for over 95 years. Tripp Lite´s innovations include the world’s first UPS system designed specifically for personal computers and the world’s most trusted premium surge protector—the Isobar®—with more than 19 million in use. Tripp Lite maintains the highest level of ready-to-ship inventory in the industry with more than 4,000 different products, including UPS systems, rack systems and cooling solutions, PDUs, PowerAlert® software for enterprise-level system management and control, surge protectors, KVM switches, cables and connectivity products, inverters, power strips and notebook accessories. Headquartered in Chicago, Illinois, Tripp Lite maintains a global presence with fully staffed offices worldwide. Additional information, including a list of Tripp Lite’s sales offices and authorized reseller partners, can be found by visiting Tripp Lite’s website: www.tripplite.com.

Over 95 Years of Manufacturing Excellence
Tripp Lite: Everything But the Server

www.tripplite.com • 1.773.869.1776