RELEASE NOTES PowerAlert Network Shutdown Agent 12.5.0 11-FEB-2022 Copyright (c) 2022 by Tripp Lite All Rights Reserved IMPORTANT NOTES * This version of PowerAlert Network Shutdown Agent software, herein referred to as "PANSA", is supported by the following Operating Systems: Windows 7, 8, 10 (32 & 64 bit) Windows Server 2008, 2012, 2016 (32 & 64 bit) REQUIREMENTS * Refer to the PowerAlert Network Shutdown Agent User Guide for details. DEFECT FIXES PANSA-40 PANSA discovers PAL with community 'tlremote' but then never receives traps PANSA-67 shutdownesxi.sh does not work if called using PANSA (but does manually) PANSA-68 shutdownesxi.sh script seems to incorrectly send extra shutdown command and/or hard shutdown VMs PANSA-70 "[: vm-xxxx: unary operator expected" errors when running shutdownvcenter.sh scripts PANSA-71 PANSA does not properly handle PADM20 connections PANSA-73 Typos/omissions in comments PANSA-102 PANSA reports "status" as severity of highest unacknowledged alarm even if there are no active alarms PANSA-106 Cannot update or install PADM when PANSA is installed ENHANCEMENTS KNOWN ISSUES END RELEASE NOTES